NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi,We use STM32WB15CC for our projects and some MCU's FUS version are 0.0.0.So we want to try re-program FUS file to MCU.While we checked STM32CubeWB, there are FUS files for STM32WB3x and STM32WB5x in "STM32WB_Copro_Wireless_Binaries" folder, but no...
"Using SPIRIT1 to transmit packets. I need an empty command (like NOP). Will it be generated automatically, or do I need to add it manually? I didn't find any relevant explanation in Datasheet. Also, can FEC be manually disabled?"
I am trying to upgrade my Nucleo board to Wireless firmware stack v1.17.0 from GitHub (Address: 0x08021000), but I always get the Warning:FUS_STATE_ERR_UNKNOWN after upgrading.And when I try to start FUS, I get:Error: FUS_STATE_ERR_UNKNOWN: Unknown e...
Hi.I am working on a ZigBee project for the STM32WB55. I use Zigbee wireless binary of STM32Cube_FW_WB_V1.16.0 as below.stm32wb5x_Mac_802_15_4_fw.bin, stm32wb5x_Phy_802_15_4_fw.bin, stm32wb5x_Zigbee_FFD_fw.bin. It works well for now with using zigbee...
Hello, who can tell me if I did something wrong?really confused why it´s not working at all after I built and flashed the application on astra1b board.Wireless stack: stm32wb5x_BLE_Stack_full_fw.binselect the example customUCchange settings to genera...
Is the WLCSP49 functionality same as that of UFQFPN48 package? Due to size reduction and I assume fewer contact pads in the former, I'd like to know if there are any functionality differences between the two. We are currently validating the possibili...
Hi, I was working as usual with my NUCLEO WL55JC1 board, powered from external 3.3V. Everything was working correctly and I turned the power suplly off, after turning it on again (next day), the board didn't work. I know the program is not runnin be...
Hello,Thank you for your detailed answers. I have resolved the design concerns related to this.I need your input for another issue. I am working on upgrading the wireless stack & FUS programmatically. I am NOT doing the OTA firmware upgrade but stori...
Hello,Is it possible to increase the size of UUID in iBeacon_data from 16Byte to 64Byte?Thanks
I'm trying to use Range 2 mode in my custom STM32WB55 board to reduce power consumption in my board.I found the protocol that switchs Range 1 to Range 2 mode in RM0434 document.The basic protocol is like below and I found that three register should b...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.