STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WLE5 Sigfox credentials for production

Hi,I have a working sigfox prototype based around a STM32WLE5. The generation of the Sigfox ID and PAC has so far been done by uploading the chip certificate (236 bytes at 0x1FFF3F04) to https://my.st.com/sfxp to get the credentials back. This proces...

Resolved! Reduce power consumption in STM32WB55

I'm trying to develop an STM32WB55-based BLE wireless circuit.I designed a custom STM32WB55 circuit and I found that the circuit consumes ~ 7 mA when 32 MHz clock and BLE fast advertising mode.Unfortunately, my circuit should allow 7 days of continuo...

KKIM.6 by Senior II
  • 4080 Views
  • 4 replies
  • 2 kudos

Example to generate 2.4GHz carrier wave signal

Hi Support, we want to be able to generate a 2.4GHz Bluetooth carrier wave to test our hardware.Is there a sample project or a sample .hex file I could use to do this.Also pointing me to the correct documentation to achieve this would be greatly appr...

SRoop.1 by Associate
  • 1754 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.