cancel
Showing results for 
Search instead for 
Did you mean: 

Stm32wb55rev6 communication with custom zigbee3 client

niko27
Associate II

I have a zigbee 3 client working on channel 11 . But It was developed by some other person who was not in touch anymore .. the issue is I need to develop a project that only read a temperature data and frequency value and send those 2 values over zigbee client that connected on a PC through a TTL .. I don't have any idea about zigbee communication procedure and API s . And also I didn't got any source where I can easily understand the process .. can  anybody give. Some guidance to do th process

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STTwo-32
ST Employee

Hello @niko27 

I suggest you to take a look to the following application notes:

Also, you can also refer to this wiki and all his sub-categories for more informations.

Then, you can refer to the Zigbee examples of the STM32WB cube package.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.