NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi, I'm working on a project involving 2.4GHz RF communication and I am considering using the STM32WB series alongside the BlueNRG-1. I'm looking into the compatibility of these two devices, especially regarding the use of ST's specific drivers. My q...
Looking to migrate our design from the SPBTLE-RF to the STM32WB1MMCH6. Our application is running on a separate MCU communicating with the module using the HCI & ACI doing BLE communications. Has anyone done this migration, or know if the modules ...
Dear support team, I was trying to build a thread device with a nucleo-wb55rg board. I did the following steps:- Implement Full chip erase- Upgrade firmware STM32Cube_FW_WB_V1.17.3\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB5x\stm32wb5x_Thread_F...
Hi,I'm new to Zigbee and STM32WB55, and I need to retrieve certain electrical measurement attributes through Zigbee Server and Client communication. While examining the electrical measurement header file (zcl.elec.meas.h), I observed that some attri...
I would like to do peer - peer stuff and experiment with LoRa.....Question: Do I use the LoRaWan stack when I am doing peer - peer, or is that strictly used when I want to communicate to a gateway?Is there literature that explains all the settings i...
I'm starting using BLE Mesh on Nucleo wb55rg, I've seen the STM32CubeWB Package and in it there are tools for getting started with a BLE mesh Network. Following the steps in this wiki I get a small error.I'm uploading code for Friend NodeI'm uploadin...
Hi everyone, I have a project to send a struct to receiver Lora from transmitter Lora. I have searched almost all sources to use Lora with STM32CubeIDE while using a library or not, but I couldn't send a data anyway. Can someone help me about this pr...
I have 2 NUCLEO-WL55JC1 boards I am using to communicate using LoRa. The Tx board sends a message every 10 seconds, the Rx board receives the message and lights up an LED..I have this working at SF7, the same spreading factor as the ping-pong exampl...
I have been stuck on the OTA using BLE. I have understood how to change the linker file in STM32 Cube IDE(Flash. ID) and I have most of my code written by my team on arduino ide(basically it is BLE Application). Now my problem is that I am unable to...
I have an STM32WB55 Nucleo Pack and i thought i'd try out the BLE heartbeat monitor example on the MB1355C board, so i opened up the STM32CubeProgrammer, put the power selector to USB STL and could connect ok.I Selected the hex file for the heartbeat...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.