2023-12-12 7:33 AM
I'm using a micro stm32wl55 (RAK3172). I try to shut it down using shutdown mode. By turning it off without ever using the PWR_SUBGHZSPICR command, the micro turns on and off regularly with the expected consumption. However, if I activate the PWR_SUBGHZSPICR command even just once, after the shutdown the consumption remains high and I can no longer turn it off completely. Could you give me a solution? Thank you
2024-01-05 6:06 AM
Hello @lino
The command PWR_SUBGHZSPICR doesn't exist. But we have the PWR_SUBGHZSPICR_NSS which I used to perform testes on Low_Power_Modes using an STM32WL55JC1 Nucleo Board. Everything works Fine. Can You give more details.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.