2023-12-13 1:44 AM
Hello,
I'm trying to flash \STM32Cube_FW_WB_V1.18.0\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB1x\stm32wb1x_BLE_Stack_full_fw.bin at address 0x08021000 with SMTCubProgrammer version 2.14.0
I think that it is unsuccessful, and the application BL2_p2pClient failed to run.
10:24:05:288 : Reconnected !
10:24:05:288 : Success with Time elapsed during Reconnect: 1172 ms
10:24:05:288 : r ap 0 @0x20002F04 0x00000004 bytes Data 0x410FC241
10:24:05:288 : fail @0x00000001
10:24:05:288 : Warning: FUS_STATE_ERR_UNKNOWN
10:24:05:288 : r ap 0 @0x20002F04 0x00000004 bytes Data 0x410FC241
10:24:05:288 : fail @0x00000001
I have also encountered the same error "failed to reconnect after starting FUS operator"
and I have read the post "Problem FUS when I try to load BLE Stack on STM32WB15xx" from JCALD.1
To follow instruction in "https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32WB_BLE_Hardware_Setup", I need a FUS file, but I did not find anything for STM32WB15CC in \STM32Cube_FW_WB_V1.18.0\Projects\STM32WB_Copro_Wireless_Binaries\STM32WB1x directory.
So, how to solve my problem? My NUCLEAO-WB15CC is out of order...
Thank you for help.
Best regards
FWX.
2024-01-05 7:26 AM
Hello @FWX
I was able to flash this .bin file to the specific indicated address on the STM32WB15 Nucleo board. I suggest you take a look at this post and follow it after performing a mass erase.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.