STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

FUS bug with ZigBee firmware for STM32WB55CGU6 (dongle)

Hey, everybody!I looked at the Release Notes for the STM32WBxx Copro Wireless Binaries and kind of did everything according to the manual.stm32wb5x_FUS_fw.bin -> 0x0809A000, tm32wb5x_Zigbee_FFD... -> 0x0804C000. However, after flashing the controller...

Fur by Associate
  • 3066 Views
  • 4 replies
  • 0 kudos

Wireless stack on custom STM32WB55

Hi all,Im trying to load the stack onto the custom board. I've done it for both Nucleo board and dongle. I use Nucleo board with SWCLK, SWDD, RST, GND, 3V3. I think Ive managed to program FUS as it shows the correct number and it starts. Ive been try...

DWuje1_0-1704136897434.png DWuje1_1-1704137140186.png DWuje1_0-1704138322460.png
DWuje.1 by Associate II
  • 4971 Views
  • 3 replies
  • 0 kudos

STM32WB15 test BLE Tx in custom hardware

Hello, I'm Marco, HW developer.Scenario: two Nucleo WB15CC transmit both a sawtooth into the Nucleo WB55 USB dongle with BLE protocol. With a proper SW we can see the two sawtooth in the GUI. The Nucleos WB15 should be replaced with custom HW with sm...

MFail.11 by Associate III
  • 869 Views
  • 0 replies
  • 0 kudos

Unexpectedly small L2CAP fragment size in BLE data transfer

I'm working on a BLE application which uses a pair of BLE characteristics to transfer packets of data (similar to a cable replacement service). I believe I have followed the recommendations in AN5289 8.6.9 to mazimize throughput.When I read packets f...

crwper by Senior
  • 2990 Views
  • 2 replies
  • 0 kudos

Increase STM32WL Range

Hello , I'm using the Nucleo-WL55JC1 in my project as Gateway and End-devices.The SW Works well and it communicate properly, but i have problem with the RANGE between the Gateway and the End-device.Know when I change the Antenna I can communicate wit...

PCB Design / Programming Interfaces for STM32WLE5C8U6

Hello,I'm interested in using one of the STM32WL chips for a telemetry board. I need this board to be as small as reasonably possible. I am trying to decide on a way to program it and (optionally) have a way for it to connect to a laptop via usb. Ide...

Mystical by Associate
  • 1322 Views
  • 1 replies
  • 0 kudos

Power WB55 via 5V Pin and have USB connected at the same time

Hi,is it safe to interface a WB55 via USB and simultaneously power it via the 5V pin from some external batteries? The battery-voltage I use is limited to 5V. I have some concerns about bricking some electronics due to multiple grounding. Are there s...

XG by Associate II
  • 4803 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.