NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello all, I have been running into a lot of issues trying to get the firmware for the BLE onto my board using the STM32WB55RG. Now I did follow this video and originally got it working, but then I accidently hit delete firmware and was unable to get...
Dear Team, I am using STM32WBA5MMG in my project. The datasheet does not contain pin description and their alternate functions. I also checked STM32WBA5xxx datasheet (DS14127). It does not contain any pin description and alternate functions of STM32W...
I have an X-Nucleo-67W61M1 with a Nucleo-WB55RG host board. I was following this link for how to do the set up How to use X-CUBE-ST67W61 STM32CubeMX pack. One of the prerequisites says that I need to ensure that I flash the updated code before using....
HERE WE R USING STM32WB55 MCU FOR BLE PURPOS AND FACING ISSUE IN FLASHING BLE STACK .HERE IT SHOWS 0.0 STACK VERSION AND FUS VERSION 2.1 IN IMAGE AFTER READING. WE ARE USING ADDRESS FOR FUS 0X80EC00 AND FOR BLE STACK WE ARE USING 0X80C7000 OR 0X80C0...
I am using the Stm32wb09kev6tr ic for the ble.I am not able to update the fus or wireless stack from the st link? is there anything i am doing wrong? is there any documents regarding this which will helpfull?
When I Debug cmwx1zzabz_0xx, I get a hard fault somewhere near a call to HAL_PWR_EnterSLEEPMode(). It happens just after all the init code, somewhere in the first call to MX_LoRaWAN_Process(). If I step into MX_LoRaWAN_Process() and continue stepping...
I enabled the bonding feature in STM32WB5MMGH6TR.Bonding is working correctly. But when the device(STM32WB) is bonded to phone(Android 15), calling disconnect from the phone does not disconnect the device.This problem does not occur when:-1. Phone An...
Hello ST Community,I am working with NUCLEO-WBA55CG and encountering a startup issue when using the BLE_p2pServerThreadX example from STM32CubeWBA v1.8.0.EnvironmentBoard: NUCLEO-WBA55CGMCU: STM32WBA55 (single-core Cortex-M33)SDK: STM32CubeWBA v1.8.0...
FUS and BLE update.I would like to know if it is possible to update FUS (1.2.0)(2.1.0) and BLE (1.23.0) via SWD. I need to update two boards simultaneously and am having problems with programming via DFU. One of the boards always shows an error. I us...
I'm currently working on an STM32WB project and would appreciate guidance on the correct sequence to enter STOP2 low-power mode and wake up via an EXTI interrupt, ensuring all peripherals resume normal operation post-wake-up.Specifically, I’m looking...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.