STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WL RTC

Hello There i am using https://github.com/STMicroelectronics/STM32CubeWL/tree/main/Projects/NUCLEO-WL55JC/Applications/LoRaWAN/LoRaWAN_End_Node_FreeRTOS this example ,in that there is timer used for sent the data , i want RTC for send data for partic...

Schematic Review STM32WBA5MMGH6TR

I am using STM32WBA5MMGH6TR in my project for sending data received from a sensor. BT is used for transmission.The data will be transmitted to a central node.This is a battery operated device. The signal chain is given below.Sensor--> ADC-->STM32WBA5...

Hariom by Associate III
  • 397 Views
  • 2 replies
  • 1 kudos

Boost stm32wl5moc lora range

Hi,   I'm working with LoRa on STM32WL5MOC for a custom board and comparing performance with the dev board. I've measured RSSI and SNR at different distances. - Custom board vs Dev board RSSI, SNR values are noted for reference. How do I improve the ...

STM32WBA5MMG: What happens when BOOT0 is high?

Split from STM32WBA5MMGH6TR Debug interface PCB layout - which is a separate question.Hi , thank you very much.In my module (STM32WBA5MMGH6TRTR), there is only one pin for boot selection BOOT0. I believe when it is pulled low booting happens from mai...

Hariom by Associate III
  • 252 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WBA5MMGH6TR Debug interface PCB layout

I am using STM32WBA5MMG in my design. This the development board schematic. Below image is from development board schematic.As per the constrains , SWDIO and SWCLK must be length matched. Also need to provide a shield.My questions are given below.SWD...

Hariom_1-1768823941790.png
Hariom by Associate III
  • 407 Views
  • 3 replies
  • 1 kudos

STM32WL5MOC Custom Board Power Consumption Too High

I have tested the LoRaWAN_End_Node example on a B-WL5M-SUBG1 board and I measure power consumption of 1.7uA when the processor is in STOP mode between transmissions.  This is exactly what I expected to see.I designed a very simple custom board based ...

JHCarter by Associate III
  • 757 Views
  • 3 replies
  • 0 kudos

STM32WBA5MMG BOOT0 pin

Dear Team,How to configure the BOOT0 pin of this module.In the reference design it is let floating with an option to pull up.In the application note (How to develop RF hardware using STM32WBA MCUs - Application note) it is pulled down.May I know in a...

Hariom_0-1768403083920.png
Hariom by Associate III
  • 554 Views
  • 6 replies
  • 2 kudos

Resolved! STM32WL30 Reference Design

The Application circuits in the Datasheet under section 5 do not list any values for the components, are they available somewhere? All of the reference designs linked in the wiki and on the website are for the STM32WL33C. Do the values directly trans...

Tobias3 by Associate II
  • 598 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.