2026-01-13 10:21 PM
Hello ST Community,
I am working with NUCLEO-WBA55CG and encountering a startup issue when using the BLE_p2pServerThreadX example from STM32CubeWBA v1.8.0.
Board: NUCLEO-WBA55CG
MCU: STM32WBA55 (single-core Cortex-M33)
SDK: STM32CubeWBA v1.8.0
RTOS: Azure RTOS ThreadX
Example: BLE_p2pServerThreadX
IDE / Toolchain: IAR Embedded Workbench 9.60
Debugger: ST-LINK (on-board)
After programming the firmware to the board:
:cross_mark: On cold power-on (Power-On Reset), the application does not start
:white_heavy_check_mark: After pressing the RESET button, the application runs normally
The issue is 100% reproducible
BLE advertising starts correctly only after a manual reset, not after initial power-up.
The issue occurs even when Timebase Source is set to SysTick
The MCU is confirmed to be STM32WBA55 (single-core)
(not STM32WB, no wireless coprocessor)
No user code is executed after early initialization during the failing POR case
After RESET, behavior is normal without any code changes
During the failing Power-On Reset case:
HAL_GetTick() always returns 0
SysTick interrupt does not appear to be running
BLE initialization seems to stall during early startup (likely in timebase-dependent code paths)
During the RESET case:
SysTick is correctly enabled
HAL_GetTick() increments as expected
BLE stack initializes and advertises normally
This strongly suggests that SysTick is not properly enabled or reinitialized after POR, possibly due to the interaction between:
HAL_Init()
ThreadX low-level initialization
BLE initialization using HAL timebase–dependent APIs (e.g. HAL_Delay() or timeout loops)
This appears to be a startup sequencing issue specific to Power-On Reset when using:
CubeWBA v1.8.0
ThreadX
IAR 9.60
SysTick may be left disabled or misconfigured after POR, while a manual RESET correctly reinitializes NVIC and SysTick state.
Is this a known issue in STM32CubeWBA v1.8.0 with ThreadX projects?
Is there an official workaround or patch recommended by ST?
Should SysTick be explicitly reconfigured before tx_kernel_enter() in WBA ThreadX applications?
Has this issue been fixed in a later CubeWBA release?
Any confirmation or guidance would be greatly appreciated.
Thank you for your support.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.