STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Issue on Bluetooth in STM32WB5MM

Hello all,  In my Project I'm using STM32WB5MMG Mcu for Bluetooth via data transmission, Iam Developing code as per the reference of STM32WB5 Nucleo Board and ST's MOOC for Bluetooth pairing,single data read and write.Iam doing as same as the Nucleo ...

image.png image.png image.png image.png
Kavinraj by Associate III
  • 1010 Views
  • 1 replies
  • 0 kudos

STM32W55 - UART DMA only odd byte is received

Hello,I have a BLE application and I want to use UART DMA for communication between Nucleo and PC.I have managed to get it working, however everytime only odd bytes are received. (One is received and the second one is not and again..) I'm attaching a...

LPTIM wb55 issues with HAL_LPTIM_AutoReloadMatchCallback

Hi community,I'm having some issues with LPTIM on a WB55 nucleo board.I have set a LPTIM to fire interrupts every 2us (with a PWM output). It uses PLL as CLK source, and the PWM signal I see in output is effectively correct.The problem arises when I ...

BANIDA_0-1714492275615.png
BANIDA by Associate
  • 1148 Views
  • 0 replies
  • 0 kudos

Using L476rg and sx1272MB2DAS

I'm developing an end-node based on the STM32 Nucleo-L476RG with a LoRa module SX1272MB2DAS and a Grove sensor (based on DHT11). I'm facing a dilemma regarding how to retrieve data from the sensor. I'm torn between two options: modifying the data ret...

ABA by Associate II
  • 4013 Views
  • 7 replies
  • 3 kudos

STM32WLE5JC: naming convention for timer?

I also found programming by serial line in below using STM32F446.  Does STM32 has a 'naming convention' for timer, (Like, Basic, Enhanced, etc....), such that I can 'quickly' see if the timer inside our STM32WLE5JC target MCU will have the 'link/slav...

David_ by Senior
  • 1139 Views
  • 0 replies
  • 0 kudos

WB55RG BLE Beacon Example via HCI only

Dear All,I am search for an example BLE beacon code for the NUCLEO-WB55RG board which solely uses the HCI layer.There is an example for the WBA board: https://github.com/STMicroelectronics/STM32CubeWBA/tree/main/Projects/NUCLEO-WBA55CG/Applications/B...

whati001 by Associate II
  • 1784 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WLE5CCUX 48 pin package

I am trying to enable all 3 UARTS (LPUART, USART1 and USART2) within the STM IDE. However, on choosing LPUART, USARTS2 become unavailable (and vice versa) . Is this a device limitation?   We really would like to be able to use all 3 uarts (no flow co...

DavidG7 by Associate II
  • 3632 Views
  • 6 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.