STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4119 Views
  • 0 replies
  • 3 kudos

Resolved! Disable BLE while Zigbee running

Hi, I would like to disable/re-enable BLE and keep the concurrent Zigbee stack in normal operation. Some other posts suggested to call hci_reset() to disable BLE and re-initialize it later when needed again.After calling hci_reset() somehow Zigbee wo...

Resolved! P-Nucleo-LRWAN2

Hello all,I have purchased the p-nucleo-lrwan2 set that has a gateway and a end node. In the tools and software they have mentioned how to connect the gateway with LORIOT,TTN and Acitility. But I have a requirement such that gateway and end node-1 (i...

Krithika by Associate II
  • 2604 Views
  • 3 replies
  • 1 kudos

Resolved! Serching examples for my "NUCLEO-WL55JC1"

I have found :C:\STM32WL_WS\Hands-on\Point2Point_Phy\Projects\NUCLEO-WL55JC\Applications\SubGHz_Phyand also :C:\STM32Cube_FW_WL_V1.3.0\Projects\NUCLEO-WL55JC\Applications\SubGHz_Phy\SubGHz_Phy_PingPongBut it is very difficult to work on this ... by e...

DAbad.1 by Associate III
  • 1639 Views
  • 1 replies
  • 0 kudos

Resolved! Why the STM32WBA52CG SYSCLK must be 16MHz when the BLE was enabled

HI,All    I noticed that when we use BLE stack, we must set SYSCLK to 16MHz。When i set the SYSCLK upto 100MHz,the uart1 log will be garbled after call BleStack_Init which contained in st ble stack lib。I don't know if my discovery is correct。I don't u...

Xiaojie by Associate III
  • 4087 Views
  • 5 replies
  • 1 kudos

Resolved! How/where to put option in STM32CubeIDE gcc -D_TIME_BITS=64

Is the STM32CubeIDE defaults 64 bits in unix time?  if not, how/where to put gcc command line option in STM32CubeIDE "gcc -D_TIME_BITS=64".  Supposedly, this will redirect unix time to be 64 bit instead of traditional 32 bit that will overflow in yea...

David_ by Senior
  • 2801 Views
  • 3 replies
  • 1 kudos

Resolved! Seek information pointer on Power Saving STM32WLE5JC

Would appreciate pointer and insignt on learning how to do battery minimum energy LoRa on (a) half a dozen of sleep modes (b) example sequencer C coding with power saving  (c) reading list on application/tech notes, etc.  TIA

David_ by Senior
  • 1773 Views
  • 2 replies
  • 1 kudos

STM32WB1MMC RF Layout

HelloIs there any RF layout documentation for STM32WB1MMC? Minimum ground plane size, distance to PCB edges, copper clearance etc? I can't find anything.Thanks

marc6h by Associate
  • 2088 Views
  • 3 replies
  • 0 kudos

My first project with STM32WB5MM-DK

I received my first STM32WB5MM-DK.Reeded  AN5289 first 104 pages to understand the architecture of the examples.And watched this youtube playlist "STM32WB Getting Started Series". So after importing the Heart Rate example with cubeIDE (Version: 1.14....

netanelu by Associate III
  • 1722 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.