2024-04-30 8:54 AM
Hi community,
I'm having some issues with LPTIM on a WB55 nucleo board.
I have set a LPTIM to fire interrupts every 2us (with a PWM output). It uses PLL as CLK source, and the PWM signal I see in output is effectively correct.
The problem arises when I call HAL_LPTIM_AutoReloadMatchCallback(), in which I simply toggle a pin at the same frequency (500KHz, 2us).
The representation of the signals is here below, where the first graph is the PWM signal and the other is the pin I want to toggle in the callback:
The only line of code inside the callback is HAL_GPIO_TogglePin(A0_GPIO_Port, A0_Pin);
Do some of you know why this happens?
Thanks so much
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.