2026-01-14 7:07 AM
Dear Team,
How to configure the BOOT0 pin of this module.
In the reference design it is let floating with an option to pull up.
In the application note (How to develop RF hardware using STM32WBA MCUs - Application note) it is pulled down.
May I know in all these three configurations(Pull up, Pull down, floating) what will be happening. From where it is booting.
You have any document which describes how to configure this BOOT0 pin.
Regards
Hariom
2026-01-14 12:47 PM
The BOOT0 pin determines where the microcontroller will start execution after a reset (boot mode). Depending on its logic level at reset, the STM32 can boot from:
Main Flash (user application memory)
System memory (factory bootloader: UART, USB, etc.)
SRAM (in some STM32 families)
According to the Reference Manual RM0492 and application notes for the STM32WBA series:
| 0 (GND) | Boot from Main Flash (user code) |
| 1 (VDD) | Boot from System Memory (internal bootloader) |
:white_heavy_check_mark: BOOT0 = 0 → Executes user application from Flash
:repeat_button: BOOT0 = 1 → Enters bootloader (e.g., for DFU via USB or UART)
| Pull-down (to GND) | MCU always boots from Flash (normal mode) |
| Pull-up (to VDD) | MCU enters bootloader mode |
| Floating (not connected) | Undetermined behavior / may pick up noise |
:prohibited: Avoid leaving BOOT0 floating — it can result in unpredictable boot behavior!
For final products: use a 10kΩ pull-down resistor to ensure boot from Flash.
For firmware updates via bootloader (e.g., USB DFU):
You can add a jumper or button to pull BOOT0 high before a reset.
In the schematic shown: there’s a jumper (possibly labeled DNF – Do Not Fit) allowing pull-up to VDD, which can be used for bootloader mode.
RM0492 – STM32WBA Reference Manual, see the Boot configuration section
AN2606 – STM32 Microcontroller System Memory Boot Mode (detailed bootloader guide)
AN5522 – How to develop RF hardware using STM32WBA MCUs (mentioned in the question)
2026-01-14 1:05 PM
@Alexandre__Promont Please don't post AI slop answers. This one in particular is incorrect in many ways. If you don't want to or can't fact check it, don't post it. Bad answers are worse than no answers.
2026-01-15 3:05 AM
I understand your concern about not making this type of publication, but I always ask questions and use AI a lot to learn, and I would like you to tell me which points are incorrect, even for my growth and knowledge with stm32.
Thank you in advance.
2026-01-15 3:29 AM
May I , know the answer for my question.
2026-01-15 5:53 AM
Consider it something you can investigate yourself to grow and learn with STM32.
2026-01-15 5:55 AM
Sure. I am exploring. Will come here if I fails.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.