STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

STM32WB5MM-DK On-board i2c sensor polling and BLE

Hello guys.I have an STM32WB5MM-DK disco board and im trying to get familiar with the ble stack. What i want to do is create a p2p server, poll an onboard i2c temp sensor for data and send that data through ble. What i did at first (successfully)was ...

AlexES by Associate III
  • 218 Views
  • 0 replies
  • 0 kudos

Nucleo-WB55RG BLE Not Working on Zephyr

Hi everyone,I am encountering an issue while trying to run the Zephyr Bluetooth peripheral sample on a Nucleo-WB55RG board.I am currently working with the Zephyr main branch (specifically commit v4.3.0-2267-g3be4c4c5a819).Hardware & Firmware Setup:Bo...

umut373 by Associate
  • 605 Views
  • 1 replies
  • 1 kudos

Resolved! X-CUBE-EEPROM adding zeros randomly to current page

Dear ST members,My application is using the EEPROM emulated library (X-CUBE-EEPROM) with an STM32WB microcontroller. I noticed that, when I update a variable, the page can be padded with random zeros. Attached are screenshots of the page before and a...

rs-dp by Associate III
  • 382 Views
  • 1 replies
  • 0 kudos

STM32WB55 is not scanning using the whitelisting

According to BLE spec, whitelisting is not related to paired or bonded devices. Our application uses the advertisement and scanning for sensor beaconing application. STM32WB55 is not able to scan the interested sensors by whitelisting. STM32WB is not...

STM32WL disable LmHandlerJoin at startup

Hi,  I'm using a STM32WL5MOC. I see that in the LoRaWAN_Init the LmHandlerJoin is not in a USER CODE section, meaning that it can't be disabled. In my application I would like to do the join upon my request and not in the init. How I can prevent from...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.