NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello, I am working on a new design using the STM32WBA52CGU6, but I have not found a specific value for the RF output impedance of stm32wba,How do I match it to 50 ohms?
Hello everyone, I have a problem with Nucleo-STM32WB55RG. I am trying to make an OTA Firmware application but for starting I am trying to make bluetooth application. I'm trying to reboot it using ST BLE Toolbox and it works good. But when I add 2 mor...
I am running into some trouble with a STM32WB while using a custom GATT server and attempting to disconnect from an Android device. The core issue is that the CPU2 has turned on the HSE. This is known because the HSERDY bit is set while the HSEON bit...
Any advice on where to start to track down an issue related to a custom BLE server not functioning on custom hardware? I am using the STM32WB35CEU6A and have flashed the firmware and wireless stack as well as followed this guide: CubeMX Initializatio...
I am attempting to connect to the STM32WBA55CG using a JLink Compact Plus following the following instructions from SEGGER: https://wiki.segger.com/ST_NUCLEO-WBA55CG.This connection fails as the DAP is not responding. The output from JLink is attache...
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
I'm trying to find out the wireless technology that I can use for peer to peer communication. The main requirement is to have good data transfer speed (at least 500kps or more), pairing process should be without user intervention and the devices will...
I have an STM32WB55CGU6 processor. I initially started with updated the FUS from v0.5.3 to v1.0.1 via the STM32CubeProgrammer. This update was successful. I then proceeded with trying to load the v1.2.0 FUS. However I got the following error:After do...
Hi Community, I tried to connect and use 802.15.4 sniffer function from CubeMonitor-RF app. I stopped at the very first step. Once I opened the CubeMonitor-RF program, it said I need to install wireshark, after install the wireshark, the warning mess...
I'm using MCU STM32WB55CE. The issue is the following:after putting MCU in STOP mode it looks like IWDG still running and reset the MCU.Option byte: 0x3B79F1AA, means bit IWDG_STDBY and IWDG_STOP clear.I'm using SEGGER J-Link for debugging. Ble stack...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.