NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello STM Community,I'm currently exploring the capabilities of the Nucleo-WL55JC1 development board and its compatibility with Amazon Sidewalk. Amazon Sidewalk is a low-bandwidth, long-distance wireless protocol designed for certain IoT devices.Coul...
Hi,I use STM32BW55.I get trouble for pairing random value.pairing random value is 0xffffffffffffffffffffffffffffffff.How do I resolve it?I set :static random addressIRERappearanceIO capability : No Input/No outputBonding Mode : Bonding ModeSecure Con...
Hi,My application (WB15CC) stays most of the time in standby mode transmitting the advertainment packet. After a couple of minutes, the advertainment packet must be updated. When I try to update the packet after waking up from the standby mode, the f...
Good dayI am using the STM32WL55 chip for a project. I did preliminary tests using the NUCLEO-WL55JC2 Development board.I created a custom PCB following the design of the Development board.When I program the custom board with the same firmware that w...
I find that when entering deep sleep/range 2 using aci_gap_set_non_discoverable(), C2 would not reliably enter the ultra low (~4uA) power consumption mode, current would jump to ~5mA. I am using stack 1.18 and even 1.19. a) Calling aci_gap_set_non_...
I have 2 devices on my SPI bus that need different CPOL settings. both use CPHA = 0 and the SPI peripheral is configured to use Motorola frame format.Communication works with both devices if their respective CPOL setting is set in CubeMX (and thus fi...
H,I just had some custom boards with STM32WB55CG and I would like to flash the BLE stack into the microcontroller. For some reason the STM32CubeProgrammer does not allow me to flash the FUS or BLE stack files, it always comes back with warning/errors...
I am developing a BLE peripheral device using the NUCLEO WB55RG. I am having trouble connecting to smartphones. The pairing process is as follows: The security is Just Work, using bonding mode.During the first pairing:The peripheral sends a security ...
I am trying to include a tinycbor .h file and as per third party include method i have done all the step but still i get the error about the linker didn't find a definition of library API functions. Here is the all the screenshot of my project and lo...
Hello everyone I've encountered an issue with connecting to Linux, specifically Ubuntu 22.04, while the Linux device is acting as a BLE gateway running the Bleak python library to manage connections. The firmware used was loosely based on the instruc...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.