STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

HeartRate with FreeRTOS

Hi Madam/Sir,I'd like to ask for help regarding creating a new Project replicating the HeartrateFreeRTOS example. When I load my custom board with the HeartRateFreeRTOS example, I'm able to connect with ST's BLE toolbox and see all the data incoming....

Resolved! Does the STM32WB BLE stack implement Security Level 4 (Elliptic Curve Diffie-Hellman Encryption)?

NIST Special Publication 800-121(https://tsapps.nist.gov/publication/get_pdf.cfm?pub_id=934038)recommends using BLE Security Mode 1 Level 4 (page v) which calls forElliptic Curve Diffie-Hellman encryption. Does the latest STM32 BLE stack for the STM3...

STM32WB10 BLE advertising not visible on other devices

Hello,I have a custom PCB with STM32WB10 with full BLE stack configured with server profile and a custom template in Cube IDE. The problem is that other devices don't see its advertising packets (or maybe are ignoring them), I tried BlueSee on a Macb...

MTkac.1 by Associate II
  • 2665 Views
  • 4 replies
  • 0 kudos

stm32wb55 SHCI_C2_SetSystemClock() causes hardfault

I find that when entering deep sleep using aci_gap_set_non_discoverable(), C2 would not reliably enter the ultra low  (~4uA) power consumption mode, current would jump to ~5mA. a) Calling aci_gap_set_non_discoverable() while there is RF activity can ...

rudivs by Associate
  • 1463 Views
  • 1 replies
  • 0 kudos

Resolved! Simple BLE advertising application

Hi there :waving_hand:I am quite new to the topic of developing BLE hardware.My goal of the current project is quite simple:I have a custom board featuring stm32wb55ceu6 and a ambient temperature/humidity sensor.All hooked up including the RF part wi...

Exeu by Associate III
  • 3923 Views
  • 4 replies
  • 0 kudos

Resolved! Which example to read, Pingpong or LocalNetwork_Sensor?

Which example 'may be' a better start for reading?  Do they use interrupt, DMA and power saving mode?SubGHz_Phy_PingPongLocalNetwork_Sensorhttps://github.com/STMicroelectronics/STM32CubeWL/tree/main/Projects/NUCLEO-WL55JC/Demonstrations/LocalNetwork/...

David_ by Senior
  • 1326 Views
  • 1 replies
  • 1 kudos

STM32WBxx & AWS IOT CORE

Dear, all.Im trying to read the trough the forum regarding information about AWS IoT Core and MCU's, same with the mainpage for STM, but the amount of information is so big, that im having some issues navigating to figure out the information i need.M...

Slakan by Associate
  • 1680 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.