2024-03-28 6:58 AM - edited 2024-04-03 6:54 AM
I find that when entering deep sleep using aci_gap_set_non_discoverable(), C2 would not reliably enter the ultra low (~4uA) power consumption mode, current would jump to ~5mA.
a) Calling aci_gap_set_non_discoverable() while there is RF activity can cause CPU2 to get stuck in a spin loop and become unresponsive.
b) aci_hal_set_radio_activity_mask(0x0002) can be used to obtain an RF event ACI_HAL_END_OF_RADIO_ACTIVITY_VSEVT_CODE
to synchronize call to aci_gap_set_non_discoverable() while no RF activity (assuming event is serviced in time; it is only in main() thread).
But even after successfully calling aci_gap_set_non_discoverable(), if CPU1 remains in run or sleep mode longer than about 200ms after
CPU2 disables advertising, again CPU2 can get stuck in a spin loop.
The above issues can occur even if using aci_gap_set_limited_discoverable(); when 180 seconds is up there is a chance CPU2 will again just spin if condition a) or b) at the time.
After lookning at https://community.st.com/t5/stm32-mcus-wireless/stm32wb55-random-core2-hard-faults/m-p/58804. Any call to SHCI_C2_SetSystemClock would simply cause a hardfault, probably incorrect clock condiguration ? again what is the expected conditions for use when callling SHCI_C2_SetSystemClock ?
There does not seem to be any supporting documentation or comments in the library for the purpose and use of this function. I have introduced this function, using the library example, into my code but now get a hardfault after calling SHCI_C2_SetSystemClock.
As a work around I would reset the entire stack and re-init with aci_hal_stack_reset() and APP_BLE_Init(). This is more reliable but after a few hours/days run time the problem would return.
2024-05-22 5:24 AM
Hello @rudivs
to avoid any problem will using the SHCI_C2_SetSystemClock(), you have to avoid calling "SHCI_C2_SetSystemClock()" from the idle task as we are running in critical section. Also, It will be a good idea to call SHCI_C2_SetSystemClock() in UTIL_SEQ_PreIdle() to switch from PLL to HSE and SHCI_C2_SetSystemClock() in UTIL_SEQ_PostIdle() to switch from HSE to PLL will using a sequencer. Finally, you have to avoid calling SHCI_C2_SetSystemClock() before receiving the ready event from CPU2 at startup or if pending.
Hope this help.
Best regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.