2023-08-02 2:44 AM
Hi Madam/Sir,
I'd like to ask for help regarding creating a new Project replicating the HeartrateFreeRTOS example. When I load my custom board with the HeartRateFreeRTOS example, I'm able to connect with ST's BLE toolbox and see all the data incoming. So I tried to create a new project, I enable the Free RTOS and the BLE too. Unfortunately, I was only able to use the BT Sig Heart Rate Sensor profile. I compiled it and load it on the Board without touching any code. Unfortunately, I cannot detect the board on my phone.
Now here is my Question, did I miss some configuration that causes my board not to be able to be detected? I was pretty sure my board is working because I have tried the HeartRateFreeRTOS example and also tried my previous custom program received from the phone which was derived from a youtube workshop and it works.
Any help would be appreciated.
Thanks,
Ian
2024-05-22 8:18 AM
Any news on this subject ? I'm trying to do the same.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.