STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Sends a packet periodically using BLE_LLD

I want to write a very simple program that sends a packet using BLE_LLD. For simplicity sake, for now, I prefer not using sequencer and put everything in the main loop.According to UM2804, I should be able to do that only using HAL interfaces. I star...

Severex by Associate
  • 1572 Views
  • 1 replies
  • 0 kudos

Resolved! Missing macro COPY_UUID_128 after changing UUID in CubeMX

Hi,When creating a custom template BLE app in CubeMX everything works fine while not changing the UUID of service1, it builds and compiles well. But if I change the UUID to my own UUID (with UUID 128 input type to full), after generating the new code...

Remyhx by Associate III
  • 3642 Views
  • 5 replies
  • 2 kudos

STM32WB5MMG problems

I made a Demo using STM32WB5MMG to communicate with USB dongle or phone (BLE notification),AND I collect data from the MAX30001 (two interrupt pins PC10 and PC11, SPI1 communication) and the MAX30112 chip (interrupt pin PD0, I2C3 communication) by tr...

Lep_0-1713755444199.png Lep_1-1713755452567.png
Lep by Senior
  • 3590 Views
  • 5 replies
  • 0 kudos

Resolved! LPM Mode does not run the radio

I have succesfully implemented my own BLE advertisement (LEGACY) using the STM32WB55 MCU.I have attached my code below.In a nutshell I have created three timers and two tasks.When the Heartbeat timer expires it calls the Heartbeat function:This then ...

BettleBerry_0-1716444093530.png BettleBerry_1-1716444228475.png BettleBerry_2-1716444287916.png BettleBerry_3-1716444322703.png

Resolved! aci_gatt_update_char_value_ext issue

Hello,We are trying to use MTU larger than 24X bytes.The characteristic size set to 483 bytes (CFG_BLE_MAX_ATT_MTU).We tried to use aci_gatt_update_char_value_ext to set the value (as the HCI layer is limited to 255 bytes transfer).aci_gatt_update_ch...

APort by Associate III
  • 2043 Views
  • 1 replies
  • 0 kudos

Low Power Mode in STM32WB

           I am using STM32WB for My Application, I want to initailly mcu is stop mode or sleep mode,when external interrupt (switch) is triggered its wakeup from low power mode.After wake up re-installize the System Clock for Mcu running configured ...

PRIYA_En by Associate
  • 2311 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.