STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WLE5J Lora

Hi  I am using the module Lora-E5 which has the STM32WLE5J inside.  Looking at cubeMX , I can select LoraWan, but I want to only use the Lora side. Do I simply select the LoraWan, and use the Lora part, as it requires LoraWan key etc which I wont use...

Issue with APP_LOG exceeding 256 bytes in STM32WL55JC

I am Using an STM32 WL55Jc  i.e., STM Nucleo Board and  I am using an example code that is https://github.com/stm32-hotspot/STM32WL-SubGHz-Phy-Rx-Hop Here in this code  APP_LOG(TS_ON, VLEVEL_L, "OnTxDone\n\r");Issues that i am facing with APP_LOG met...

Resolved! Issue with Data Interference between BLE and SPI Communications

Hi. guys.I'm trying to make BLE communication to PC with the SPI interface to the analog-front-end in my custom stm32wb55 board.However, I found that the transmitted data through BLE to PC appears in SPI received data (RX).So, can anybody explain why...

KKIM.6 by Senior II
  • 2020 Views
  • 2 replies
  • 0 kudos

Resolved! X-CUBE-Matter unable to add to CubeIDE 1.14.1

After downloading en.x-cube-matter-v1-0-3.zip and attempting to install from a local folder, as CubeIDE 1.14.1 nor 1.15.1 have it listed as a package yet.It asks for the .zip or .pack file, shortly after selecting the zip file I get the message as in...

AlecDavis2021_0-1716412604221.png

Resolved! STM32WBA52 about LSI2 question on STM32CubeMX

Hi,Got a new MCU with LSI2 from the distributor. I want to use it for the 2.4 GHz RADIO sleep timer, but can't find LSI2 register settings in STM32CubeMX.Additionally, I'm curious why the STM32CubeWBA version V1.3 doesn't support the STM32WBA52 serie...

1714441720229.jpg
CY_Tsai by Associate III
  • 2377 Views
  • 2 replies
  • 0 kudos

Resolved! STM32WB OTA SCB->VTOR

Hi,I need to add OTA functionality to a CubeMX generated project. The readme.txt file from the BLE_HeartRate_ota project has a note saying "Remove the update of SCB->VTOR in the file system_stm32wbxx.c". On my current CubeMX generated project the SCB...

rs-dp by Associate III
  • 1613 Views
  • 1 replies
  • 1 kudos

How to use USB/UART/BLE stack with sequencer?

I have problem with USB stack as Virtual Port COM to use it with sequencer prepared to BLE stack. I mean I don't know how to execute needed CDC... functions inside usbd_cdc_if.c. Did anybod do that?I want to send via UART and via BLE received through...

_legacyfs_online_stmicro_images_0693W00000dJpIoQAK.png
dnj by Associate III
  • 1525 Views
  • 1 replies
  • 0 kudos

BLE server stops adverstising

Good afternoon....I have a known working board with an STM32WB5MMGH6TR (server).  I am using an apk on a google pixel 6a.  The application scans for the device and if not found has a re-scan button that user can hit to try and connect (I am not the w...

SWenn.1 by Senior III
  • 1671 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.