2023-06-01 4:48 AM - edited 2023-11-20 4:13 AM
I have problem with USB stack as Virtual Port COM to use it with sequencer prepared to BLE stack. I mean I don't know how to execute needed CDC... functions inside usbd_cdc_if.c. Did anybod do that?
I want to send via UART and via BLE received through USB VCP.
Any Application Notes to do that?
2024-05-23 11:36 AM
Hi @dnj
USBD_CDC_ItfTypeDef defines the interface for CDC class on firmware. Each of the functions corresponds to a callback that should be called during operation. As far as I know, to implement a CDC VCP with sequencer, is like implementing it in as task in an OS. The following example does not use an OS:
I hope this would be helpful
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.