STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Bluetooth module without pairing

Hello,actually, i'm searching some reference of Bluetooth module without pairing, i want that the Bluetooth module communicate directly without paring.Can you give some references please ?Thanks

ljm by Associate III
  • 6456 Views
  • 15 replies
  • 0 kudos

How to make a BLE obscerver

I try to make an obscerver with a p-nucleo-wb55 that scan the surounding and give the adress id and the RSSI.  I used the project P2P client as a base and add some codes : In the app.ble.c file in the SVCCTL_App_Notification function i add in the cas...

Xourel by Associate
  • 2226 Views
  • 3 replies
  • 0 kudos

Optimize power

How does the STM32WB/ STM32WBA optimize power consumption during audio playback in BLE-enabled devices?

Tom_Gean by Associate II
  • 1925 Views
  • 2 replies
  • 0 kudos

Resolved! RF Communication with Nucleo-WL55JC Boards - Seeking Guidance

 Hello ST experts,I am a beginner with the STM32WL series and need some support.So first I started with the STM32F407VG disc1 and I tried to communicate two boards of it using a SI4432 module and I didn't succeed, I tried something else and I bought ...

Zayoud_0-1714992026470.png Zayoud_1-1714992085220.png Zayoud_2-1714992269586.png Zayoud_4-1714992348239.png
Zayoud by Associate III
  • 15730 Views
  • 10 replies
  • 7 kudos

Cell chemistry advises for Lora

There are quite a number of cell chemistry for Lithium (and possibly others).  Which one is good for Lora:Transmit time of 1.5 seconds or less, current 1C or less. Recharge 0.5C to be safe (may be 1C on spec.).Normal (non transmit) low duty cycle loa...

David_ by Senior
  • 1245 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WB55CGU6 Example for Home Automation

Hello, I'm trying to get Zigbee working on my STM32WB55CG6 custom board. I've verified that the RF section works since BLE works perfect but now I'm trying to get Zigbee working. Since there aren't alot of examples I've tried the Zigbee_OnOff_Server_...

Resolved! STM32WB about BLE

Hello,I made 2 project about client and server using stm32wb1mmc product. > server project is using "custom p2p server"It works well but I want to improve usability. 1. How to reduce scan time for connect client to server?  > I quote it from examples...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.