2026-01-21 9:58 PM - last edited on 2026-03-02 7:26 AM by Imen.D
Hello,
Board: NUCLEO-WL55JC2 (2 boards)
MCU: STM32WL55JC
IDE: STM32CubeIDE
Programming: Bare-metal C or Cube IDE(C/C++)
Goal:
I want a minimal RF example using two NUCLEO-WL55JC2 boards where one board transmits a simple message and the other receives it and for example toggles an LED .
I searched on ST website and GitHub, but most available examples are full LoRaWAN stacks. I could not find a simple RF Tx/Rx reference similar to an LED blink example.
I have not written RF code yet and am looking for an official ST reference to start from.Suggest any website reference or youtube videos where i can understand it clearly.
Questions:
1. Is there an official ST RF Tx/Rx example for NUCLEO-WL55JC2?
2. Any recommended CubeWL example or GitHub repository?
3. Which example is best for learning basic RF communication?
4. Should i need to use the RF like NRF24L01 Transcever or does it supports?
Thanks in advance.
2026-01-23 1:53 AM - edited 2026-01-23 1:59 AM
Look for the "Ping-Pong" example: that's a simple peer-to-peer link using only LoRa modulation - no LoRaWAN network.
PS:
I think the LoRa Ping-Pong example is in I-CUBE-LRWAN;
There's also one for the Sub-Ghz PHY STM32CubeWL:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.