2026-01-21 2:31 AM - last edited on 2026-01-23 2:08 AM by Andrew Neil
I just flashed the end node of the P nucleo LRWAN 3 with the AT master firmware, but I am still unable to send AT commands via my terminal to reconfigure some parameters of the end node. I also made sure I set up all the necessary parameters in the terraterm software correctly and I am still not able to communicate with the end node via terminal using AT commands.
2026-01-23 2:08 AM
IIRC, 'AT Master' is the one where the STM32 is sending the AT commands to an external LoRa slave device.
So the AT commands are not for you to control the system ?
again, the P-NUCLEO-LRWAN3 is marked as NRND - and probably should be marked Obsolete.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.