STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB Correct approach for low power using BLE sequencer

Hello,I am developing a custom BLE app on a custom STM32WB55CEU6 board.I need it to periodically (every x seconds) wake up from stop2 mode, read FIFO of a sensor, process the data, go back to stop2 (CPU2 is advertising in the meantime). When a user c...

STM32WB5MM-DK unable to start USB bootloader

Dear ST team, I have an issue with starting the USB bootloader with the STM32WB5MMG-DK and I am sure it is for lack of knowledge. The AN2606 states the following: and USB pins should be able to function as the following:The pattern 16 looks like like...

FDumontKeller_0-1714999492263.png FDumontKeller_1-1714999581304.png FDumontKeller_2-1714999745402.png FDumontKeller_3-1715000251529.png

STM32WB persistent user data region after OTA update

Hello,We are working on a device based on a STM32WB5MM. The module has configured the SBSFU, the BLE OTA and the user application.We have defined some sections in the flash memory to store device data, like the serial number or the pin code used for ...

STM32WB5MM OTA Application at a different address

I have multiple questions:1. Is there a limit on the firmware size in STM32WB series? If yes, what is the limit?2. Is there a limit on the firmware size of the OTA application in STM32WB series? If yes, what is the limit?3. I want to perform OTA at a...

Lalit1 by Associate
  • 1248 Views
  • 1 replies
  • 0 kudos

STM32WL5 2nd core reset

Hi,I'm using STM32WL5 SoC in my lora project.I started from this example: "LoRaWAN_End_Node_DualCoreFreeRTOS".In my board, I have a problem at startup, CPU2 doesn't start after a simple pin reset (NRST).The only way is to switch power supply off, wai...

DiegoKer by Associate
  • 1168 Views
  • 1 replies
  • 0 kudos

BLE Connection issue on p2p Client

Hello all,         In my project I'm using STM32WB5MMG MCU for BLE Server and Client.BLE Connection between p2p Server and p2p Client is working well but I want connect Custom Templete Server with p2p Client.In this case Server and Client are not con...

WhatsApp Image 2024-04-25 at 3.41.54 PM.jpeg WhatsApp Image 2024-04-25 at 3.14.00 PM.jpeg
Kavinraj by Associate III
  • 1289 Views
  • 1 replies
  • 0 kudos

How to factory reset ASTRA1B

Hi,Bought online  ASTRA1B  previously used,  for school project,I do not have experience with  ST Boards.Need Help with following:where to find stock firmware (default factory firmware)  ?Do I need STLINK-V3MINIE for flashing firmware ?How to factory...

Resolved! Costum board stuck at PeriphCommonClock_Config();

hi, Im using my own costum board with a STM32WBA52CG on it. When I'm nog using the RF my code is working perfectly. When I activate the RF in the STM32CubeIDE, my code is stuck in  PeriphCommonClock_Config();More specifically in the following code: I...

Screenshot 2024-05-07 at 17.34.13.png
matsmort by Associate II
  • 2674 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.