STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

HCI_COMMAND_COMPLETE_EVT_CODE cannot be received

BLE peripherals are implemented using NUCLEOWB55RG.I would like to check if Advertsing is working properly by receiving the completion of the asynchronous aci_gap_set_discoverable execution with HCI_COMMAND_COMPLETE_EVT_CODE, HCI_COMMAND_COMPLETE_EVT...

STM32WL DAC Sample-And-Hold: Internal capacitor?

I want to generate a constant, steady voltage as COMP INPM in STOP1 with the DAC (using HAL libs at the moment).Unfortunately I cannot get a steady signal. The voltage drifts around some seconds, stabilises and starts from the beginning (oddly seems ...

surumadurum_0-1713209445540.png

SIGFOX_API_start_continuous_transmission

Using this API returns 0x3157 error code after running SIGFOX_API_close successfully (return code is 0), anyone tried that? What are we missing here?BTW - Same behavior observed when using ST provided Sigfox_AT_Slave_DualCore example out of the box w...

ASchw.1 by Associate II
  • 2332 Views
  • 4 replies
  • 0 kudos

Resolved! STM32WL55 dual core debug _ error 18 when debugging CM0+

Hello,I have started to use stm32wl55 nucleo.I try to debug a basic application.I start by debugging CPU1 (CM4) than after booting CPU2 (CM0+) i run the debug for the second CPU.But ST-LINK: Could not verify ST device!error details :Error in final la...

malarab by Senior II
  • 16447 Views
  • 16 replies
  • 0 kudos

Possible values for ACI_GAP_IS_DEVICE_BONDED response packet

Found below what I assume to be the Possible Values for 'Status' , but not sure, any other? 0x5C Device not found in DB0x5E Device not bonded Can you list all of them?Or are those values in the Bluetooth Specification? If so can you provide a link?  ...

DS4_0-1715167703983.png
DS.4 by Senior II
  • 1897 Views
  • 3 replies
  • 0 kudos

Where to go next with STM32WB using the B-U585I-IOT02A

Hello,I've been recently starting to get into the STM32 ecosystem using the B-U585I-IOT02A discovery board, first by toggling LEDs and GPIOs but eventually trying to get familiar with how to use the integrated STM32WB5MMG module.I was able to get a d...

LocalNetwork Demostration problem

Good morning,I am using two NUCLEO WL55JC1 development boards and the LocalNetwork_Sensor and LocalNetwork_Concentrator example that I found in the development software provided by ST. When I use a frequency band of 868MHz and a bandwidth of 125 KHz ...

Software_Problem.jpg
Henry77 by Associate II
  • 1326 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.