cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB5MM OTA Application at a different address

Lalit1
Associate

I have multiple questions:

1. Is there a limit on the firmware size in STM32WB series? If yes, what is the limit?

2. Is there a limit on the firmware size of the OTA application in STM32WB series? If yes, what is the limit?

3. I want to perform OTA at a different address, not 0x08007000. Is it possible?

 

 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
STTwo-32
ST Employee

Hello @Lalit1 

I suggest you to take a look at the recommandations of the AN5247 and the following MOOC. They should be the best guides for your questions.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.