NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Sto usando questo microcontrollore stm32wl5moc e in particolare il core M4. Uso due funzioni in linea per leggere e aggiornare i valori delle mie variabili. Accesso alle variabili tramite puntatori. Quando sono in modalità di debug su Live Expression...
I am trying to implement a multicast LoRa Class 'C' network using the STM32WL.using Chirpstack.I have created multicast group in Chirpstack and i am sending messages from chirpstack using/api/multicast-groups/{group_id}/queue.But I am not getting an...
Hi, For my project I need to put a MCU STM32WLE5CCU6 in standby mode and configure several wake-up type : Wake-up pin 1 on PA0RTC wake-upRadio wake-up on a LoRa message received by the embedded Sub-GHz radio module of the MCU with the bit EWRFIRQ (re...
I've try and I think I understood STM32WB HeartRate Exemple and on a Nucleo board it works perfectlyI can go to stop2 and keep active advertising on CM0 and keep being connectable and it wakes CM4 when connection happensbut when I try on my own app i...
Hi,I have a bluetooth keyboard. Obviously for the keyboard to be detected and used we need a bluetooth dongle and an OS that provides a bluetooth stack. This causes that at boot time the bios (UEFI), not having, bluetooth stack, is unable to detect m...
Hi everyone.im trying to create a project with a LoraWan module that based on stm32wle5ccu6.(RAK3172).after compliting my ioc UI i build the project, on the building process i got this error./LoRaWAN/App/lora_app.c:33:10: fatal error: adc_if.h: No su...
I'm Developing a RF based communication between two LORA developments kits of STM32,Part.no:b-l072Z-LRWAN-1.I was using the USB stlink for a long time for debugging it.But suddenly the Built in STlink is not working.The Stlink LED(LD5) is toggling ...
We are using the STM32WB55MMG SIP module for a simple BLE application and came across the following behavior.The application is configured to use LSE as the clock source for RTC with medium drive capability as recommended by the data sheet. The LSE f...
Hi all,we're working on a project that involves the STM32WB5MM module that is supposed to provide OTA Update.While we got the ST OTA second stage bootloader firmware to work (including our application firmware), we encountered a couple of things:For ...
Dear All,I am sharing the log from STM32cubeide and STM32cubeprogrammer. I need your help to figure out what went wrong. after debuggingI face this problem of not being able to connect to stm32wl. So I "full chip erase" is only option, then I being a...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.