STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WL33 support in STM32CubeIDE

Hi Folks, I'm fancy of the STM32WL33. But it is yet not supported in the STM32CubeIDE 1.15.1. Is there an Add-On or when will it be supported? Thanks in advance

Resolved! S2-LP searching for library and examples

Hi, where can I find the S2-LP chip library and examples on C. Also does STM provides any protocols with open code for frequency hopping and mesh based on sub-1 GHz external radio chip?  I've found just sw package with gui to configure radio S2-LP an...

AKali by Associate II
  • 1672 Views
  • 1 replies
  • 0 kudos

Resolved! Error: FUS_STATE_ERR_UNKNOWN: Unknown error

Hello, I am using a P-NUCLEO STM32WB Bluetooth 5 and 802.15.4 Nucleo Pack including a USB dongle.While trying to update the FUS of the USB Dongle to set up a Thread network, I encountered several errors.Initially, I was able to connect in DFU mode, b...

Screenshot 2024-05-22 143244.png Screenshot 2024-05-22 143334.png Screenshot 2024-05-22 143537.png Screenshot 2024-05-22 144025.png

Resolved! STM32WB5MMDK (Discovery Kit) - Configuration of the BSP example

Good morning,I am a beginner with the STM32 tools. I am working with the STM32WB5MMDK (Discovery Kit).To understand how it works, I decided to use the BSP example, but I can only see the code. I don't have a .ioc file that I could run with STM32CubeM...

Nour by Associate III
  • 2254 Views
  • 4 replies
  • 0 kudos

LoRaWAN_End_Node_DualCoreFreeRTOS stops transmitting

I have a "working" demo of the LoRaWAN_End_Node_DualCoreFreeRTOS. I have it connected to a gateway and see a new payload every 10 seconds as expected. However, it stops transmitting after so long (usually 2-3 minutes). All I can tell is I get an I...

AParr.2 by Associate
  • 1151 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.