STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB55 Nucleo Pack FUS Upgrade Fail

HelloThe Nucleo/Dongle pair did not do the demo.So downloaded and updated them with P2Pserver and Client hex files.Still didn't work.Am now trying to upgrade the FUS in the dongle from .53 to current using stm32wb5x_FUS_fw_for_fus_0_5_3.bin, using 0x...

GRama.2 by Associate III
  • 6624 Views
  • 7 replies
  • 1 kudos

Resolved! STM32WBx5: available Flash and SRAM when using BLE

I am developing an application based on a STM32WB35CE and have noticed that the code generated by STM32CubeMX limits available Flash to 256k and available SRAM to 32k (the WB35CE has 512k and 96k, respectively). I have flashed the stm32wb3x_BLE_Stack...

Resolved! MB1791 Bill of materials

Hi Sir. Madam,​For MB1791 Development Broad, there are 3 Type of ​design:MB1791-HighBand_HighPowerMB1791-HighBand_LowPowerMB1791-LowBand_HighPowerBut I doubt the BOM given, the part Description, Value and Manufacture Part Number are not tally for the...

0693W00000bhSADQA2.png
KKan.1 by Associate II
  • 2441 Views
  • 5 replies
  • 0 kudos

Resolved! BSP example - Configuration - Ressources

Hello everyone,I am working on a STM32WB5MMDK. I already posted a question about the BSP example.I have few other questions about it.I wanted to replace the Button 1 by the Button 2 so I changed it in the main file (even the CallBack). I checked the ...

Nour by Associate III
  • 3528 Views
  • 6 replies
  • 1 kudos

Resolved! MuRata CMWX1ZZABZ Variants

Hi,Many of the MuRata CMWX1ZZABZ variant support "Opne MCU" such as the -078 variant; meaning the STM32 chip is programmable. Appearently some do not have the "Open MCU" feature even though they use an STM32. Was hoping someone could clear why this i...

Resolved! Master and Slave Project on B-L072Z-LRWAN1

I'm new to the ST development Environment and it is my first time to be using embedded systems. My aim is to make a project of one master that communicate with multiple slaves. I have already tried the ping pong example with 2 B-L072Z-LRWAN1 boards a...

Sondos by Associate II
  • 2604 Views
  • 4 replies
  • 1 kudos

Resolved! STM32WB p2p Client could't p2p Server?

   Initially Iam flash 2 binary files to STM32WB5MMG (stm32wb5x_FUS_fw.bin & stm32wb5x_BLW_Stack_full_fw.bin ) in that case p2p Server works with ST BLE Toolbox in mobile but in my project p2p Client as another MCU.p2p Client not working well its can...

Kavinraj by Associate III
  • 2411 Views
  • 4 replies
  • 0 kudos

Sync Word for Modem Lora

 Hello ST Community,I am currently working with a STM32WL 55JC  and I need assistance with setting the sync word for both the transmitter and receiver. Here are the details of my setup.Here I have configured my module to USE_MODEM_LORA and these are ...

doubt1.JPG doubt2.JPG doubt3.JPG doubt5.JPG
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.