NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello all. I am trying to integrate STM32 with Sx1262. But I am facing issues and not able to find a perfect example code. I am using https://github.com/Lora-net/sx126x_driver?tab=readme-ov-fileBut the issue is my implementation. Please someone help ...
I AM USING STM32 WL55JC2 CONTROLLER(NUCLEO-WL55JC2) TO WORK AS A LORA END NODE ,I AM TRYING TO TRANSMIT ANY DATA WITH UART2,I AM WORKING IN A SEQUENCER FUNCTION ,APP_LOG(TS,VL,...) IS A FUNCTION THAT IS LINKED WITH UART2 WITH DMA TRANSMIT, WHERE I AM...
Does not appear to be an appropriate label for my question. I can't find schematic for this board so I can map pins. I read that this info is in user guide, but don't see it listed in user guide for the board here: https://www.st.com/en/evaluation-t...
Hello,I wish to know if it possible to have references of all the boards and devices around STM32WB on this link because I wish to buy it please and the application to do work it ?https://www.youtube.com/watch?v=eqAFVi16l5EThanks a lotRegards
When Debugging the code in STM32 Cube IDE, the program execution flow directly goes into the HardFault Handler. The Debugging starts at HardFault Handler and I don't know why? Also this happened when I am trying to interface Sx1262 LoRa Module with S...
Hi,i am currently trying to read out VBAT of a STM32WB55CGU6 Board (Custom).VBAT is connected to a 3V Battery, and all other VDD pins are connected to the same battery since the board is only powered by this battery.I have setup ADC1 and enabled the ...
Regarding the standby mode of the STM32WB5MMG, I have enabled only the RTC wake-up as trigger to wake up every second.However, occasionally it freezes in standby mode, and after a watchdog reset, it doesn't even perform initialization processes.Final...
When combining the standby and OTA samples (listed below), in some cases, the OTA sample is started at the timing of standby wakeup.・PWR_STANDBY_RTC・BLE_OtaIn my understand, whether the standby or OTA sample is started is determined by the first 4 by...
HI, I am using STM32WBA55G-DK1 board to develop ble audio device. When i call CAP_EnableAudioCodecController, it return 0x91. I have reviewed the assembly code of the project and found that CAP_EnableAudioCodecController will call hci_read_loca...
For our validation:I would like to verify my computation for the capacity of the bonding list size. I did have some characteristics created so it's not the default , but its a number close to that. ( Sources in the bottom) It would be disastrous if e...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.