NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi, I use an STM32WB with the BLE stack. In my code, I need to write data to the flash memory (writing new firmware to a prepared memory area). Unfortunately, when I attempt to write to the flash, an error occurs. Is there anything special that I nee...
Hi, I have a STM32WBA55G card and I want to flash an example code but it doesn't work. So I used STM32Programmer to find out why my board wasn't "found". Normally STLink is included and I can go through the usb-c port. But I still get an error if I ...
I have configured a BLE MESH with two nodes one as client and other as server . It is working well . I also want to recieve the same data that is being exchanged on Phone. Can someone tell me how this can be done and what app I must use.
I bought ST-LINK/V2 from a certified reseller, and I have WIO-5E mini with STM32WL5JC from [Seeed.com](https://Seeed.com) on the board. This WIO-5E was already programmed by another ST-LINK/V2. I connected WIO-5E to ST-LINK as required. I want to rep...
I try to debug on a STEVAL-IDB011V1 with WISE Studio.Whatever I try with any project, I have the same error when the debugger tries to launch:Open On-Chip Debugger 0.11.0+dev-00062-g6405d35f3-dirty (2021-03-26-11:44)Licensed under GNU GPL v2For bug r...
I have two stm32wb5mm dk configured as mesh server and client . I used example BLE_MESH_MODEL_SENSOR. Can someone tell me what file mentions the data that is being sent and how can I add external sensor or a way to add external service so that it ca...
Hello everyone , I am try to learn lorawan on a STM32WLE5 module, I am using this repository(https://github.com/Seeed-Studio/LoRaWan-E5-Node/tree/main/Projects/Applications/LoRaWAN/LoRaWAN_End_Node) for developing lorawan application. It works well b...
HI ,I am trying to flash the STM32WB55CGU6TR using i2c bootloader mode.I can successfully get into the bootloader mode and able to read the bootloader version.But while performing the Erase operation its get failing(Time out Error).I am writing the b...
Hello.I have a question while using two examples(BLE_Audio_TMAP_Central, BLE_Audio_TMAP_Peripheral) provided in STM32Cube_FW_WBA_V1.4.0.This example provides voice communication via BLE.In this process, I want to transmit voice communication data via...
I've been struggling to connect my nucleo board via ST-Link, I've tried uninstalling everything, reinstalling and my computer still won't detect the board when I plug it in. It's always just COM-3 device or whatever port I use. Tried installing the S...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.