2024-08-02 8:30 AM - edited 2024-08-02 8:32 AM
I have two stm32wb5mm dk configured as mesh server and client . I used example BLE_MESH_MODEL_SENSOR. Can someone tell me what file mentions the data that is being sent and how can I add external sensor or a way to add external service so that it can be utilised. Also how can I limit the number of nodes required because i need to use just these two and a smartphone which should recieve the data.
2024-08-09 8:36 AM
Hello @Rituraj
I suggest you debug the original BLE_MESH_MODEL_SENSOR to understand how it works. You can also take a look at the AN5292. Also, you can refer to this wiki. Some research on those Resorces should do the job for you.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.