NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hi All, I am trying to get a custom BLE and MEMS project running on the Nucleo-WBA52CG board - however looks like the STM32_WPAN middleware does not work properly also in the latest WBA software pack the applications folder for the board does not hav...
I am designing a project using custom hardware that utilises the STM32WB55 to stream ADC values via DMA from which I want to process using a python script for gesture detection. I want to minimise the use of peer to peer communication and omit the us...
When running second core initialization, the program goes into HardFault on line "i_feature = *(i + p_MBMUX_Cm0plusFeatureList->Feat_Info_TableAddress);" The code was automatically generated by CubeIDE when opening the ST program "SubGHz_Phy_PingPong...
Hi,I am trying to make a simple BLE service with a custom characteristic descriptor and UUID (128 bit) has anyone got any good examples of this?The reason I ask is when I running a BLE server to advertise the characteristics always just seem to show ...
Hi, I'm trying to use the STSAFE-A110 to store my LoRaWAN keys, to generate session keys and to encrypt my payloads through it.I'm supposed to send commands to the secure-element but for the symetric encryption, neither the datasheet nor the source c...
Has anyone encountered the issue that external loader works fine only when flashing QSPI EFlash_Section independently (e.g. slice the firmware.elf into MCU.bin and EFlash.bin and flash separately).BUT if flash from 0x08000000(Complete Firmware) the ...
Hello,Our IoT product is LoRa based, and uses the STM32WLE5JC mcu. For the purpose of operability in several countries, we have used a Molex antenna, which operates in the frequency range 863MHz to 928 MHZ.We're using the STM32CubeIDE for development...
Hi all,no experience, so please explain like to a child.I want to jump into digital.My idea is to make a bluetooth speaker with LED meter so:USB C for Power(CYBD3177) and/or Audio IN(STM32wb5).Bluetooth Audio IN (STM32WB5) -> out to Class D Amp (TAS5...
Is NUCLEO-WB55RG/WB15CC compatible with X-NUCLEO-PLC01A1? I want to develop a controller that supports BLE and thought of starting with a combination of these two boards. Would be helpful if someone can confirm that these boards are compatible and ca...
Hello. Thanks again for all your appropriate assistance.I would like to ask a question about the implementation details of BLE_Hid in STM32CubeWB.> Is the data written by aci_hal_write_config_data saved in NVM area?(Is that implementation already in ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.