2026-02-23 8:33 AM
Hey guys I am currently looking for an mcu to get started developing a live stream camera board which should be in 7x80 mm dimensions what mcu should I get ? I think 5x5 footprint should be ok but not sure 6x6 also be ok. I am open any advice also new to hardware design so thanks for all the supports
:)
2026-02-23 8:37 AM - edited 2026-02-24 2:28 AM
You've posted in Wireless MCUs, so presumably you want something wireless - but what protocol(s) ?
Also, what video specs ?
How to write your question to maximize your chances to find a solution
2026-02-24 1:26 AM
Hello @Emircan and welcome to the ST community,
You need to describe the scenario of what you are trying to do so we can help efficiently.
2026-02-24 8:18 AM
Hello,
I’m building a compact smart-glasses prototype. I need either:
live video streaming (low FPS is OK), or
taking photos for a few seconds and sending them over Wi-Fi.
My main constraint is size: the electronics must fit inside the glasses temple.
Target dimensions: height < 7.5 mm, and I’m trying to keep the PCB as small as possible.
Most Wi-Fi MCUs with DVP camera interface I found are 7×7 mm packages, which makes the design difficult.
Do you have any recommendations for:
smaller Wi-Fi MCU/module that can interface with a camera (DVP or SPI), or
a compact camera module solution suitable for tight mechanical constraints?
I’m also considering a two-board approach: one board near the ear side (MCU + Wi-Fi + power), and a small second board near the lens side (camera), then i could connect them somehow
Any guidance or parts suggestions would be greatly appreciated.
Thank you.
Best regards,
Emircan
2026-02-24 8:49 AM
ST doesn't have any wireless MCUs with WiFi.
ST's only WiFi device is the ST67W coprocessor series.
You could use that with an STM32, or a 3rd-party MCU.
STM32 selection tools:
STM32 and STM8 product finder for desktops
STM32 product finder for mobile devices
You can also do a search in STM32CubeMX.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.