2026-02-19 7:48 AM - last edited on 2026-02-27 1:06 AM by Imen.D
I am trying to bring up the GFX01M2 on a WB55RG board. Following any of the Custom, FlashLoader, or HelloWorld applications (from the X-CUBE-DISPLAY_3-0-0 download) using STM32CubeIDE merely results in a blank LCD.
I feel I'm missing something simple, but just can't find it. In each case I have compiled and loaded the files as per the ReadMe instructions.
Any pointers appreciated...
Solved! Go to Solution.
2026-02-24 8:44 AM
The combination is supported in TouchGFX version 4.25.0 (and presumably later)
2026-02-19 8:14 AM
@DavePfz wrote:on a WB55RG board
Just to be clear, that is a Nucleo-WB55RG board - yes?
2026-02-19 8:20 AM
Yes. The specific combination (I tend to be lazy!) is NUCLEO-WB55RG and X-NUCLEO-GFX01M02.
2026-02-21 11:48 AM
In examining the code, I think I see the problem. The specific code at:
C:\ST\X-CUBE-DISPLAY_3-0-0\Projects\NUCLEO-WB55RG\Applications
calls out the ST7789V controller.
The datasheet for the Displaytech DT022CTFT says that it uses the ILI9341 controller!
My first thought was to simply substitute the corresponding files, but I find it's not that simple. Can someone point me to code that implements the ILI9341 on the NUCLEO-WB55RG board?
Thanks.
2026-02-24 8:44 AM
The combination is supported in TouchGFX version 4.25.0 (and presumably later)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.