STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! Newbie questions to get started with ST

Hi all,I'm new to ST and was a Nordic device users.Few questions before jumping into ST.My need is to build a radio based remote control (not BLE), that means a transceiver for TX on one side and RX on the other one.Also mandatory: Digital and Analog...

SteveJ by Associate II
  • 1837 Views
  • 3 replies
  • 1 kudos

Sigfox Backend Not Assigning Token to Registered Device

Hello Everyone,I hope you are doing well.I am currently testing the Sigfox_AT_Slave example from the STM32WL repository. My end device is configured with an ID, PAC, and Key for the South Africa region (RC = 1), as provided by the Sigfox build team. ...

Taksh by Associate III
  • 1019 Views
  • 1 replies
  • 0 kudos

STM32WB stop advertising

Hello, I am working on a BLE project with the B-WB1M-WPAN1 development board.For connection and testing, I am using the ST BLE Toolbox.For connection between the central (my phone) and peripheral (STM32WB), the pass key option is enabled, with IO cap...

Fyapie by Associate
  • 1129 Views
  • 1 replies
  • 0 kudos

sample project of STM32WB5MMG

Hi, there our new product needs STM32WB5MMG module to establish BLE and Zigbee link, also want to support BLE mesh and Zigbee mesh, so my question is  do we have a sample project which can help us to know how to build these wireless feature?  we hope...

Batch of Dead STMs received?

(Referencing forum post: STM32WL + ST-Link = Target no device found (Custom Board))My team recently ordered a set of STM32WLE5CCU6 from Digikey for a LoRa Radio project of ours. We got the PCBs manufactured from a local vendor and began assembling ou...

Resolved! Can't build STM32WL FUOTA example with STM32CubeIDE

Hi,i'm trying to run example of LoRaWAN FUOTA firmware, but build attempt ends with fail. It looks like running postbuld.sh script fails, but it only gives an information about 4 errors without any comment.After run ./build.bat I got following logs:#...

meloon by Associate II
  • 4027 Views
  • 6 replies
  • 0 kudos

Resolved! Working with aci_hal_tone_start WB55

Hi, I am trying to check the oscillator tuning of our boards and did some reference testing with a WB55 Nucleo. using aci_hal_tone_start. Using 0,0 I do get an output near 2.402GHz, but not quite were I would expect it. The header says the following:...

OliM by Senior II
  • 1266 Views
  • 1 replies
  • 2 kudos

STM32WL55 doesn't work with 1.8V

Hi,I am working on a LoRa application with the STM32WL5MOC module which features the STM32WL55JC microcontroller. According to the datasheet, this module is compatible with a voltage level as low as 1.8V.I am using the STM32CubeWL MCU Package for the...

SMav by Associate II
  • 2719 Views
  • 6 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.