NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am trying to make sniffer for STM32WB BLE application work, (ref: https://wiki.st.com/stm32mcu/wiki/Connectivity:STM32_Sniffer_for_BLE_Setup_guide). I am stuck at step 4.1. I am unable to get "STM32WB sniffer interface" on Wireshark. I tried uninst...
Dears.I am following the guide for the matter part of the stm32 wiki. I am requesting help because an error occurred in the 1.2.2.4 Matter code generation chapter.https://wiki.st.com/stm32mcu/wiki/Connectivity:Matter_develop_and_prototype#Matter_code...
I have two projects one was created some time ago with STM32CubeMX V6.10.1 and it shows me having 'blue' Enable CSS button for the LS mux the other is created with STM32CubeMX V6.12.1 (using the same exact part) YET it is greyed out. How do I change...
I am using the above subject Nucleo. I create a project and let STM32CubeIDE V 1.16.1 create a default project. I make NO changes to this. I close the .ioc and open main and add the following code (seen by Red Bars). I build and load to target. ...
Hi Sir,I run BLE_p2pServer example code with NUCLEO-WBA55CG board, it shows build error on STM32CubeIDE. How to fix it ?The software version I used is :STM32CubeIDE 1.17.0STM32Cube_FW_WBA_V1.5.0STM32CubeMX 6.13.0
I am working on a custom board with the STM32WB55 microcontroller.The BLE_Ota and Main APP software are functioning properly.However, when the microcontroller jump to from Ble_OTA to the Main APP, the advertising stops.When I remove the BLE_Ota softw...
Hello, I am developing a temperature measurement system which consists of a coordinator and multiple sleepy end devices. On the Coordinator Side ZbZclAttrReportConfigReq is used to set end devices reporting interval. To ensure the sleepy end-devices ...
Hi, I am facing issues with upgrading fp-atr-astra1 version 0.1.2 to the latest firmware update, which is 2.0.1. What I do is I directly upgrade the firmware using the Android app "The Ble Sensor." I upgraded by selecting a file called "STMicroelectr...
I currently have a product that uses the STM32WB55 microcontroller, and we have developed a phone app that has all of the user interface to the product, and it also performs OTA updates.I'm working on a new product and I'm considering the STM32WB0 se...
Greetings I have a STM32WB55 P-Nucleo board, with the STM322B55 dongle. I am trying to flash the beacon project onto the nucleo board. I have downloaded the STM32WB repo from the github linkI unzipped the file and selected the .project from the follo...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.