STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WL33 6LoWPAN

Hi, STM32WL33 is part of 6LoWPAN products, but in Firmware package there are no examples for 6LoWPAN. Can someone explain how to incorporate 6LoWPAN in STM32WL33 series ?

faruk by Associate
  • 12004 Views
  • 4 replies
  • 1 kudos

End Device HardFault after switching to ClassC

Hello,I'm working with Actility as server, on a NUCLEO-WL55JC as the End-Device. I have the STM code from the STM32obeWL repository, version 1.3.0. When running a FUOTA campaign from the server the last update sent from the end device in the serial p...

oronshifman_1-1734872265199.png oronshifman_2-1734872930882.png oronshifman_3-1734873163308.png oronshifman_4-1734874171808.png

Resolved! B-WB1M-WPAN1 P2P Server .ioc Example Not Working

Hi all, I have a brand new B-WB1M-WPAN1 board which worked with the ST BLE Toolbox out of the box. It had 2 services, Heart Rate and LED. I was able to turn the LED on and off, notify the phone with the button and see heart rate. Imported into CubeMX...

Connor48 by Associate II
  • 1535 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeIDE Prebuild step does not work

Hi All,1. [Part Number] STM32WL33CC12. [Environment] Windows OS, STM32CubeIDE version 1.17.0, Firmware package STM32Cube FW_WL3 V1.0.03. [Schematics] STM32 Nucleo-64 development board4. [Details] See below.5. [Expected behavior] The script would patc...

ola_1-1737558664198.png
ola by Associate III
  • 2111 Views
  • 2 replies
  • 3 kudos

Stm32wb55cgu6 HAL_PWREx_EnterSHUTDOWNMode();

  I am developing a very energy-efficient device. Which will work on the 2032 element. I understand that this will be a server that will wake up every 3 seconds for a short time and wait for a connection to it. I have a problem that in the HAL_PWREx_...

Resolved! How to detect BLE stack version from bin file

I have file stm32wb5x_BLE_Stack_full_fw.bin how can I understand which stack version of it file without CubeProgrammer.Probably exist doc where described of bin file structure. Or somewhere in file should be this information.

Aliaksei by Associate
  • 1326 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.