STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 301 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4118 Views
  • 0 replies
  • 3 kudos

Resolved! RTC current time in milliseconds (display in 6 byte hex)

Hello,I am using an STM32WB55 and am trying to figure out how to get the current time including milliseconds using an RTC and display that time in 6 byte hex format. I would most likely call the GetTime() based of a millisecond timer if that is the ...

kcire L. by Associate III
  • 6806 Views
  • 3 replies
  • 4 kudos

Advice for Adding cellular connectivity

I have a dev_kit which I want to use to connect to a cellular network with LTE-M. But the example-file that they gave were a .bin file from XCUBE_CELLULAR for B-L462E-CELL1\cellular. Since I never used i, I have no clue what to do. How could I get st...

Fates by Associate II
  • 1608 Views
  • 1 replies
  • 0 kudos

STM32WB09KE ble disconnect with 0x08 reason

hi ST support teamI am designing a circuit using the STM32WB09KE chip.However, when running the BLE_p2pServer example program from the package STM32Cube_FW_WB0_V1.1.0 and using the ST BLE Toolbox app (on iphone) to connect, I encounter a continuous d...

Screenshot 2025-01-21 at 00.28.54.png Screenshot 2025-01-21 at 00.41.36.png Screenshot 2025-01-21 at 00.38.26.png

STM32WB standby mode WKUPx

I'm working with the p-nucleo-wb55, and I would like to configure the pin PA0 , PC13 to wake up the MCU from Standby Mode. I configued PA0 and PC13 from STM32CubeMX to GPIO_EXTI0 and GPIO_EXTI13 respectively.Config:PA0 : External Interrupt with Fall...

jirdom by Associate II
  • 4833 Views
  • 6 replies
  • 0 kudos

Resolved! Pin sharing problem with SWD and SPI3, GPIO

Hi. I'm developing a custom board using STM32WB09TEF7TR microcontroller.I had a problem re-accessing the microcontroller using SWD once I finished programming one time.I found that it is due to the SPI3 (PA3) and one GPIO pin (PA2) sharing the pin fo...

KKIM.6 by Senior II
  • 1069 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.