2024-12-22 12:24 AM - last edited on 2024-12-27 4:25 AM by Imen.D
The simple DMA_MUX_RequestGen example code doesn't work as expected.
I have tried running the example from https://github.com/STMicroelectronics/STM32CubeWB/tree/master/Projects/P-NUCLEO-WB55.Nucleo/Examples/DMA/DMA_MUX_RequestGen
on the P-NUCLEO-WB55 board, but it does not run as expected; when I press the SW1 button, the LED2 gets on, but it stays on forever, and it does not toggle as expected (the DMA gets only the first trigger and then stops functioning)
The DMA ISRs also don't get triggered in any case.
After enabling the EXTI line4 interrupt and changing the HAL_DMA_Start_IT(&DMA_Handle, (uint32_t)SRC_Buffer_LED2_Toggle, (uint32_t)&LED2_GPIO_PORT->ODR, 2);
to: HAL_DMA_Start(&DMA_Handle, (uint32_t)SRC_Buffer_LED2_Toggle, (uint32_t)&LED2_GPIO_PORT->ODR, 2);
Somehow, it started to work, but none of the DMA interrupts will work in either case.
Then I tried configuring it with the CubleMX but I can't get it to work, the DMA gets the first trigger from the GPIO but it doesn't continue running as expected.
Basically I would expect that example code provided by STMicrocontrollers would work out of the box without any modifications?
Any help would be appreciated!
Solved! Go to Solution.
2025-01-22 10:40 AM
Hello @EM_Embedded
I've tested personally using the last version of the STM32CubeWB V1.21.0 and I've been able to make it work as it is (without modifications on the code).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-22 10:40 AM
Hello @EM_Embedded
I've tested personally using the last version of the STM32CubeWB V1.21.0 and I've been able to make it work as it is (without modifications on the code).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.