NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I have Stm32wb55Cgu6 board from from WeAct, With default FUS (V1.2) and BLE stack everything was okay. But when i upgraded the FUS 2.0 and newest BLE stack Full 1.22.1 . the Upgrade was successful, But I didn't got any Bluetooth connection for same c...
Hello,I upgraded from CubeIDE 1.17 to 1.18 and from WBA 1.5.0 to 1.6.0 and now I get this error the following error. I have logging disabled in WPAN configuration and no IP selected for logs under platform settings tab.../Core/Inc/app_conf.h:291:2: e...
[moved to MCU Wireless category -- p.]Hi Community,I'm quite new to the FreeRTOS and STM, so this might be hopefully only a beginners mistake.I have designed a small PCB with a STM32WLE5CCU6 to learn a bit in regrads of LoRaWAN. Now I'm already chall...
EDIT - cant find a way of deleting this, all resovled wont be changin names of thinsg in such a cavalier manner again! I renamed a project in CubeIDE but now I'm trying to open the project I get resurce does not exist even though I can clearly see ...
Hi, I use stm32wb09 microcontroller to build a project. Whenever I try to program from cubeIDE with stlink, I encounter with this given error on photo. With open OCD debugger selection I can program the microcontroller, but I want to program with my ...
Hi,BackgroundWorking on STM32WB55.Flash size is 1MByte.Attached .ld file describes: Boot, Bank 0 (App1), Bank 1 (App2) and DB sections.Boot and App linker files (.ld) are quite similar from memory management aspect.App .ld file /* Specify the memory ...
We have a STM32WB module soldered on custom board. Initially everything was working fine, we were able to dump code using UART bootloader and SWD. Suddenly, it stopped connecting using STM32CubeIDE and it is only connecting using STM32CubeProgrammer(...
Hello Everyone,Does STEVAL PROTEUS-1 Support BLE Mesh protocol? Is there any pre existing solution for a BLE Mesh network with STEVAL PROTEUS-1 for custom applications or HAL documentation I can reference? Thanks in advance.
Dear ST expertsIf we want to use tcxo on stm32wl33, should we choose 1.8v or 3v3 power domain for the vcc of this tcxo?
Technical Description of LPUART Communication Error Configuration: STM32WLE5 LPUART operating with LSE (Low Speed External) clock sourceConfigured baud rate: 9600 bpsTo measure the TX signals, a minimal firmware created by CubeMX was used to rule ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.