2026-05-23 11:30 AM - last edited on 2026-05-26 7:10 AM by Andrew Neil
Hi, I'm having some issues with the STM32WB06 when trying to achieve low power consumption. I hope someone can help me solve these problems.
Issue 1: After initializing the Bluetooth protocol stack and enabling automatic connection establishment, it causes the device to fail to enter the low power state (BLE wake-up has been disabled). Is this a normal phenomenon? If not, what are the solutions?
Issue 2: Before entering the low power mode, disabling automatic connection establishment allows the device to enter the low power mode normally. However, after waking up, attempting to re-enable automatic connection establishment fails (aci_gap_start_procedure(GAP_AUTO_CONNECTION_ESTABLISHMENT_PROC, LE_1M_PHY_BIT, 0, 0)). What is the solution for this problem?
I look forward to your replies. Thank you very much!
2026-05-25 7:07 AM
2026-05-25 8:31 AM
Hello @Imen.D ,
I've read this article, but the issues mentioned in it don't seem similar to the ones I'm facing
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.