2023-03-30 12:39 PM
Hello,
I am trying to use an LCD display on my custom board. I am utilizing the Rocktech RK043FN66HS-CTG display with the STM32H7B3IIT6 MCU. When I first initialize the firmware (in debugging mode), the screen flickers once or twice (showing signs of life), but then immediately goes to a black screen and stays like that.
High Level Configuration Details:
I used this video as a general guide to make sure I got the right idea, but there are differences. However, he has the same issue during debugging that I am seeing. The screen flickers then goes black.
https://www.youtube.com/watch?v=SRQD8JMeg_k
In that video, he notes that it was due to improper initialization of the RAM that caused that issue, so I am looking there to see if something is wrong.
I am doing a single buffer strategy and the buffer location is By Address, starting at 0x24040000 (AXI SRAM2), which can handle 393.216kByte according to the reference manual.
I enabled the MPU region for that region base (SRAM 1, 2 & 3) in the CORTEX_M7.
Using the TouchGFX 4.20.0 software package in the CubeMX, I configured it as follows:
LTDC Configuration:
I am using the enable signal on the display (Pin 31) and the LCD backlight dimming functionality, which I enable at start-up with a base functionality:
HAL_GPIO_WritePin(LCD_EN_GPIO_Port, LCD_EN_Pin, GPIO_PIN_SET);
uhLCD_PWM = LCD_PULSE_STARTUP;
TIM12->CCR1 = LCD_PULSE_STARTUP;(TIM12-CH1 = PB14)
(LCD_Enable is set to PE2)
I verified that the PWM signal from TIM12-CH1 is correct, as well as the voltage level from the enable.
Schematic of my display setup is below.
With this setup, I get a screen flicker on start-up, then a black screen after that.
Does anyone know what would cause this?
Solved! Go to Solution.
2023-03-31 8:21 AM
You ned see signals as on image 7.1.3
2023-03-31 9:47 AM
Understood!
I will have access to an oscilloscope on Monday (Working from home today).
In the meantime, is there anything else you can think of to try with the firmware?
2023-03-31 10:20 AM
Remove both 10nF from DCLK
2023-04-03 10:35 AM
Hello MM,
An update. You were right! The DCLK signal was completely distorted and it was due to those 10nF capacitors. I took the design from the STM32H7B3I-EVAL evaluation board, but I made a mistake. In their design, they used a 10pF capacitor and I put a 10nF by accident.
Dumb mistake! :)
Thank you for helping me diagnose it MM!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.