2021-02-04 3:40 PM
LCD_CLK that runs XGA (1024 x 768)
Thank you for helping.
environment:
STM32CubeIDE Ver1.5.0
MCU: STM32F769BI
Board: Custum
It seems that this microcomputer supports up to XGA, but LCD_CLK for XGA is not output.
Create LCD_CLK with PLL using a 25MHz crystal.
The XGA LCD panel is instructed to use a 65MHz clock with a Typ. Value.
If fps is 60 in XGA, I think that a clock of about 65MHz is required.
When I try to set 65MHz in the Clock configuration of the IDE, the output is DC.
I haven't looked at it in detail, but it seems to be output at around 10MHz or 30MHz.
GPIO_SPEED_FREQ_VERY_HIGH is selected as the GPIO speed.
How can I output a 65MHz LCD_CLK?
Also, what is the maximum frequency of LCD_CLK that can be output by STM32F769BI?
Thank you.
2021-02-04 5:16 PM
As I recall the DSI with a 16-bit colour depth would give the clock a ceiling of around 62.5 MHz, with 24-bit 41.67 MHz
I had 1024x768 running at 57 Hz and 51 Hz on the DSI/HDMI
2021-02-07 10:02 PM
Hi Tesla DeLorean
Thank you for your reply.
In my case, I use RGB0-7, HSYNC, VSYNC, DE, LCD_CLK signals.
I would like to know the maximum frequency of LCD_CLK in this case.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.