2026-02-17 10:55 PM - last edited on 2026-03-04 3:22 AM by STackPointer64
I am testing Ethernet on STM32H723ZGT6 by transmitting UDP packets (1024 bytes) every 1 ms.
Setup / Implementation:
No CubeMX / HAL used
Fully bare-metal Ethernet driver (lwIP integrated manually)
Ethernet interrupts enabled and serviced
RX handled inside while(1) loop
Non-blocking transmit path
MPU enabled
Memory configuration:
RX pool located in AXI RAM
lwIP heap: 32232 bytes in D2_SRAM
Observed Behavior:
Eventually UDP transmit stops working
Ping continues to work without issues
Debugging shows failure occurs at:
pbuf_alloc(PBUF_TRANSPORT, len, PBUF_RAM);
After failure:
1) pbuf_alloc() returns NULL (ERR_MEM)
2) ETH->DMACSR reads 0
while (1)
{
sys_check_timeouts();
if (eth_rx_rdy)
{
eth_rx_rdy = 0;
ethernetif_poll(&gnetif);
ETH->DMACIER |= ETH_DMACIER_RIE;
}
if (sys_now() - udp_tx_timer >= 1) // 1 ms transmit interval
{
ret = udp_server_send(udp_tx, sizeof(udp_tx));
if (ret != ERR_OK)
{
printf("err: %lu\r\n", ETH->DMACSR);
}
udp_tx_timer = sys_now();
}
}
err_t udp_server_send(const void *out, u16_t len)
{
if (!upcb)
return ERR_VAL;
struct pbuf *p = pbuf_alloc(PBUF_TRANSPORT, len, PBUF_RAM);
if (!p)
return ERR_MEM;
err_t err = pbuf_take(p, out, len);
if (err == ERR_OK)
{
err = udp_send(upcb, p);
if (err == ERR_OK)
tx_sent++;
}
pbuf_free(p);
return err;
}
What could cause pbuf allocation failure after long run time while ping still works?
Could this indicate lwIP heap exhaustion / memory leak / fragmentation?
Is there anything STM32H7-specific (DMA / cache / MPU / memory region placement) that might trigger this?
Does DMACSR = 0 provide any diagnostic meaning in this scenario?
Any suggestions or debugging directions ?
~AJ
Solved! Go to Solution.
2026-02-18 6:48 AM
You could try using PBUF_ROM, which - I think - would also save you the copying time.
But then check how to set up your UDP send functions and buffer + pbuf handling.
2026-02-18 4:11 AM
Check where pbuf_free() is used for UDP sending.
I'm mostly streaming TCP packets, up to ~ 50 Mbit/s, and also over hours.
In LWIP's tcp_out.c: pbuf_alloc(PBUF_TRANSPORT, u16SegLen, PBUF_ROM), then the payload pointer is set to the custom data streaming buffers placed in OCTOSPI / HyperRam.
Each descriptor also has a pointer to the used (first) pbuf, and a custom flag field (mostly used for TCP ACK status, and PTP using UDP).
In the regularly called function EthTxReleasePackets() these descriptor flags are checked, and if there's still a pbuf assigned to the descriptor, it is freed with pbuf_free().
The PTPd (heavily modified) UDP is using pbuf_alloc(PBUF_TRANSPORT, i16Length, PBUF_RAM).
But this is used only a few times per second.
Just see that the PTP UDP send function immediately frees the pbuf after calling LWIP's udp_sendto().
And other functions (e.g. SNTP) do the same.
Don't know if that helps... good luck!
2026-02-18 4:14 AM - edited 2026-02-18 4:15 AM
@ajmw_ wrote:
What could cause pbuf allocation failure after long run time while ping still works?
Could this indicate lwIP heap exhaustion / memory leak / fragmentation?
Yes, it certainly sounds like it!
@ajmw_ wrote:Any suggestions or debugging directions ?
Instrument your memory allocation & release.
Inspect your heap when the allocation failure occurs.
Some tips on LwIP debugging here.
2026-02-18 4:52 AM
Thanks for the explanation,
In my case, I'm not using PTP or any time-sync protocol. My application only performs high-rate UDP data streaming.
UDP transmit path is
pbuf_alloc(PBUF_TRANSPORT, len, PBUF_RAM);
pbuf_take(...);
udp_send(...);
pbuf_free(...);
~AJ
2026-02-18 6:48 AM
You could try using PBUF_ROM, which - I think - would also save you the copying time.
But then check how to set up your UDP send functions and buffer + pbuf handling.
2026-02-24 9:18 PM
Hi @LCE ,
After changing the pbuf type from PBUF_RAM to PBUF_ROM, the UDP streaming has been running continuously for the last four days without any interruptions.
That said, I noticed that the TCP client in the same application disconnected during this time. I am currently analyzing the cause.
Thank you.
~ AJ
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.