STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Example on how to swipe to change a screen

Hi,for my app I would like to implement a feature to swipe to change a screen. That would probably contain a combination of GestureEvent, a handler, callback and a listener. However, in 3 hours of reading TouchGFX docs, searching through the forum an...

ZRego.1 by Associate II
  • 6142 Views
  • 7 replies
  • 1 kudos

TouchGFX 4.16.0 D-Cache flush causes HardFault...

TouchGFX 4.16.0 generated code can/will crash in HardFault if D-Cache is not enabled.This happens at least in those CPUs where there is data cache (STM32F7...).This behaviour is something new that was introduced in 4.16.0 version.This change is undoc...

KPort by Associate II
  • 3215 Views
  • 4 replies
  • 1 kudos

LCD_CLK that runs XGA (1024 x 768)

LCD_CLK that runs XGA (1024 x 768)Thank you for helping.environment:STM32CubeIDE Ver1.5.0MCU: STM32F769BIBoard: CustumIt seems that this microcomputer supports up to XGA, but LCD_CLK for XGA is not output.Create LCD_CLK with PLL using a 25MHz crystal...

Mna.1 by Associate II
  • 1797 Views
  • 2 replies
  • 0 kudos

CubeMX generates TouchGFX DMA2D with error

Hi!I am using STM32L496 on Nucleo 144 board CubeMX 6.1.1 CubeIDE 1.5.1 TouchGFX 4.16.0.After generating code with TouchGFX using DMA2D error occurs during MX_DMA2D_Init. ../Core/Src/main.c: In function 'MX_DMA2D_Init': ../Core/Src/main.c:249:14: erro...

0693W000007EEvWQAW.png
kronikary by Associate III
  • 802 Views
  • 0 replies
  • 0 kudos

Error including custom header files.

HiI am trying to include a custom Header file "LCD1602.h" along with its source file "LCD1602.c" in my project. I have also added the respective path in Project>Properties>C/C++ General>Paths and symbols. But when I build the project, the macros decl...

0693W000007E1TtQAK.bmp 0693W000007E1XbQAK.bmp
MVerm.2 by Associate III
  • 4021 Views
  • 6 replies
  • 0 kudos

Resolved! TouchGFX server problem ?

Bonjour,Since this morning, I can't create touchGFX projects with my card anymore.I have this wonderful error message.My internet connection has no problems.I reinstalled touchgfx but still the same problem.

SGROU.1 by Associate III
  • 2661 Views
  • 3 replies
  • 0 kudos

stm32f769 LTDC + DSI only 1 frame then fadeout

I'm trying to run up a display with an ILI9806E controller but although I get encouraging flickers I only seem to get a single frame and then the display fades out.I've tried turning on the pattern generator with HAL_DSI_PatternGeneratorStart(), sam...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.