2025-04-14 2:06 AM - last edited on 2025-04-21 3:52 AM by mƎALLEm
Hello everyone,
I’m working on a project using TouchGFX and I would like to know if it’s possible to display real-time curves (line graphs) that represent data coming from a sensor connected via I2C.
:small_blue_diamond: I’m using a microcontroller from the STM32 series.
:small_blue_diamond: The sensor communicates through I2C (temperature sensor).
:small_blue_diamond: I would like to visualize this data in graphical form (curves or charts) on the display using TouchGFX.
My main questions are:
Is it possible to plot real-time curves or graphs using TouchGFX?
Are there any built-in widgets or recommended methods to implement dynamic data plotting?
What is the best way to send I2C data from the MCU to the TouchGFX GUI efficiently?
Are there any examples or tutorials available?
Any suggestions, code examples, or documentation links would be very helpful!
Thanks in advance :folded_hands:
Solved! Go to Solution.
2025-04-21 3:56 AM - edited 2025-04-21 3:59 AM
Hello,
Please refer to the TouchGFX tutorial: Dynamic Graph
The temperature values need to be propagated from the hardware to the graphics in MVP model.
See also this video on ST Youtube channel.
Hope that helps.
2025-04-21 3:56 AM - edited 2025-04-21 3:59 AM
Hello,
Please refer to the TouchGFX tutorial: Dynamic Graph
The temperature values need to be propagated from the hardware to the graphics in MVP model.
See also this video on ST Youtube channel.
Hope that helps.
2025-05-12 8:15 AM
Can I display real-time graphs based on temperature sensor values on TouchGFX?
I’m working on a project that involves using a temperature sensor, and I’m using TouchGFX for the graphical user interface. My goal is to display real-time graphs based on the temperature sensor values on the TouchGFX interface.
I’m wondering if it’s possible to dynamically update graphs in real-time with the data from the temperature sensor. If anyone has experience doing this or can provide guidance on how to implement real-time graphing with TouchGFX, I would really appreciate it!
Thanks in advance for your help!
2025-05-12 8:59 AM - edited 2025-05-15 9:01 AM
Hello,
I've already provided you the answer. You need to use the Dynamic Graph feature of TouchGFX. Please read the documentation here.
Read the sensor and propagate the value from the low level software (Backend module) to the GUI over the MVP model.
See how to do it in this video.
2025-05-15 8:25 AM
Thanks for that!
Regards,
rafla
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.